MODBUS.MSGLOG

Description

Use MODBUS.MSGLOG to stop Modbus message logging. If MODBUS.MSGLOG is 1, then the AKD2G drive records all Modbus messages to and from the drive. Logs are shown using MODBUS.MSGDUMP.

The message log is cleared every time the log is enabled, MODBUS.MSGLOG starts from 0 to 1.

The message log can contain a maximum of twenty entries. If the limit of entries is exceeded then older entries are discarded.

Value

Description

0

Disabled

1

Enabled (default)

Examples

To enable logging set MODBUS.MSGLOG to 1.

-->MODBUS.MSGLOG 1
-->

To view logged messages.

-->MODBUS.MSGDUMP
(39d:21h:30m:48s): 1 242 0 0 0 6 255 3 0 0 0 4 from 10.8.232.204:62944
(39d:21h:30m:48s): 1 242 0 0 0 11 255 3 8 0 0 0 2 0 0 0 0 to 10.8.232.204:62944
(39d:21h:30m:56s): 1 243 0 0 0 6 255 3 0 0 0 4 from 10.8.232.204:62944
(39d:21h:30m:56s): 1 243 0 0 0 11 255 3 8 0 0 0 2 0 0 0 0 to 10.8.232.204:62944
-->

Context

For more information, see Message Logging.

Versions

Action Version Notes

Implemented

02-05-00-000

 

General Information

Type

Read Write Parameter

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

See Also

MODBUS.MSGDUMP

Stored in Non-Volatile Memory

No

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

MODBUS.MSGLOG

3014h

08h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

3707

1

3707 (0xe7b)

MODBUS.MSGLOG

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

MODBUS.MSGLOG

3707

Unsigned8

Read/Write

-